Everything
3.3.1 Structure of link map

The structure and contents of the link map are shown below.

Output Information

Description

Header information

Version information of the optimizing linker and time of linkage

Option information

Option strings specified by a command line or subcommand file

Error information

Error message

Entry information

Execution start address

Combined address information

Combined source files, and start and end addresses and size of continuous range data

Address overlap information

Overlapped combine source files, and start and end addresses and size of overlapped range data