Everything
3.3.5 Entry information

The execution start address is output.

The output example of the entry information is shown below.

*** Entry address ***
00000100        (1)

Number

Description

(1)

Execution start address

The execution start address is output.

However, if the execution start address is "00000000", it is not output.