Everything
11.8 Using the -delete option for linkage [Optimizing linkage editor]

When a function symbol is removed by the -delete option, its following function in the source program is not allowed to have a breakpoint at its function name on the editor while debugging. If you intend to set a breakpoint via the [Label] window at the function entrance, set the breakpoint via the [Label] window or at the program code of the function.