Everything
2.11.1.1 Change display format of values

The display format of this panel can be changed using buttons below on the toolbar.

Note that these buttons are disabled during execution of a program.

Notation

The following buttons to change the notation of a data value are displayed.

 

AutoSelect

Displays values on this panel in the default notation according to the type of variable (default).

Hexadecimal

Displays values on this panel in hexadecimal number.

Decimal

Displays values on this panel in decimal number.

Octal

Displays values on this panel in octal number.

Binary

Displays values on this panel in binary number.

Encoding

The following buttons to change the encoding of character variables are displayed.

 

ASCII

Displays character variables in ASCII code (default).

Shift_JIS

Displays character variables in Shift_JIS code.

EUC-JP

Displays character variables in EUC-JP code.

UTF-8

Displays character variables in UTF-8 code.

UTF-16 Big-Endian

Displays character variables in UTF-16 Big-Endian code.

UTF-16 Little-Endian

Displays character variables in UTF-16 Little-Endian code.

UTF-32 Big-Endian

Displays character variables in UTF-32 Big-Endian code.

UTF-32 Little-Endian

Displays character variables in UTF-32 Little-Endian code.