To move to a specified address in the disassembled text, select [Go To...] from the context menu and use the Go to the Location dialog box that is opened.
In this dialog box, follow the procedure described below to Move to a specified address.

Specify an address to which you want to move the caret.
Enter an address expression directly in the text box (specifiable in up to 1024 characters) or select an input history item from the drop-down list (up to 10 history entries).
By holding down [Ctrl]+[Space] keys in this text box, you can complete the symbol name at the present caret position (see "2.21.2 Symbol name completion function"). |