The caret position can be moved to the address at which a symbol is defined.
Move the caret to an instruction that is referencing the symbol and then click the toolbar button
.
Also, if, subsequently to the above operation, you click the toolbar
button, the caret position is returned to the instruction that was referencing the symbol before the caret was moved.