Everything
2.2.4 Delete column

The Pin Configurator is used to delete the "user's own column" from the device pin list using the [Delete Column] button in the Column Chooser dialog box that opens by pressing the button in the upper left corner of the device pin list.

To delete a column, select the column you want to delete in the displayed item selection area of the Column Chooser dialog box, and press the [Delete Column] button.

Figure 2.5

Delete Column

 

Remark

You can only delete the column which you added using the New Column dialog box.