Everything

Procedure to Create a Program

This section describes a procedure to create a program.

Start performing the task after installing CS+.

 

(1) Open the sample program

:This time, you don't use the smart configurator functions. Instead, you must read out a program from a sample program.

 

 

(2) Coding

:Since you use a sample program, you don't edit the program. Here, we describe how to perform basic operations.

 

 

(3) Build

:Build the program

(If an error occurs, edit the program again).

 

 

(4) Debugging

:Debug the program using RTK50565N2S10000BE

and E2 Lite.

 

 

(5) Writing

: Write a program to the microcontroller using E2 Lite