This section describes the manual update.
From the Windows the [Start] menu, select [Programs] >> [Renesas Electronics CS+] >> [Update Manager], or from the CS+ menu, select [Help] >> [Check for Updates...]. The CS+ Update Manager window launches.

The following image is displayed while information on the available updates is being acquired. |

A list of appropriate update items appears on the Select updates page.

Select the check boxes of updates and click [Download and install] or [Download only] in the update selection area.
When [Download and install] is clicked: (3) |
When [Download only] is clicked: (5) |
In the menu area, select a microcontroller to only display update items for the selected microcontroller. |
If Update Manager failed to obtain the information, then the Error page appears. |
Update items selected on the Select updates page appears on the Download and install page.
If there are the updates that must be installed together with the updates selected on the Select updates page, a Message dialog box appears. |

Check the information, and click the [Install] button. You must have administrator privileges to perform installation.
Update items are downloaded, and then the are installed. A progress bar on the Update in progress dialog box displays the download and install progress.
The download and install progress of each tool appear in the [Update status] area.


Go to (7).
Update items selected on the Select updates page appears on the Download only page.

Check the information, and click the [Download] button.
Update items are downloaded. A progress bar on the Update in progress dialog box displays the download progress.
The download progress of each tool appear in the [Update status] area.

See "2.5 Displaying the update history" for instructions on installing download update items later. |
When all update tasks are finished, the results of the update execution will appear on the Finish page.