This tab shows the detailed information on each file categorized by the following and the configuration can be changed.
 
(1)  [File Information]
(2)  [Notes]
[Description of each category]
The detailed information on the file is displayed and the configuration can be changed.
| 
File name | 
The file name is displayed. 
Change the file name on the project tree. | 
| 
Default | 
file name | 
| 
How to change | 
Changes not allowed | 
| 
Relative path | 
The relative path from the project folder is displayed. | 
| 
Default | 
The relative path from the project folder | 
| 
How to change | 
Changes not allowed | 
| 
Absolute path | 
The absolute path of the file is displayed. | 
| 
Default | 
The absolute path of the file | 
| 
How to change | 
Changes not allowed | 
| 
Save with absolute path | 
Select whether to save the file location with the absolute path. 
This property is not displayed if the Property panel being displayed while a dependency file is selected on the project tree. | 
| 
Default | 
No | 
| 
How to change | 
Select from the drop-down list. | 
| 
Restriction | 
Yes | 
Saves the file location with the absolute path. | 
| 
No | 
Saves the file location with the relative path. | 
| 
Last update | 
The time and date on which this file was changed last is displayed. | 
| 
Default | 
File updated time and date | 
| 
How to change | 
Changes not allowed | 
| 
Writable | 
Select whether to enable writing to the file. 
This property is not displayed if the Property panel being displayed while a dependency file is selected on the project tree. | 
| 
Default | 
Yes (when the file is write enabled) 
No (when the file is not write enabled) | 
| 
How to change | 
Select from the drop-down list. | 
| 
Restriction | 
Yes | 
Enables the file to write. | 
| 
No | 
Does not enable the file to write. | 
The detailed information on notes is displayed and the configuration can be changed.
This category is not displayed if the Property panel being displayed while a dependency file is selected on the project tree.
| 
Memo | 
Add memos to the file. 
Add one item in one line. 
The specified memo is displayed as the subproperty. | 
| 
Default | 
Memo[number of items] | 
| 
How to change | 
Edit by the Text Edit dialog box which appears when clicking the [...] button. 
For the subproperty, you can enter directly in the text box. | 
| 
Restriction | 
Up to 256 characters 
Up to 256 items can be specified. |