You can convert a CubeSuite project into a CS+ project. Select [Open Project...] from the [Project] menu with CS+, and then select a project file (*.cspj).
When a CubeSuite project file is selected, the following message dialog box will open.
![](ProjectOperation_Eng-36.gif)
If you select the [Yes] button, the CubeSuite project settings are left unchanged, and the conversion to a CS+ project is carried out.
To change the microcontroller or project name, click the [No] button (continue to (2)).
The Project Convert Setting dialog box will open.
![](ProjectOperation_Eng-37.gif)
The [Project] area shows the configuration of conversion target projects as a tree; select the project for carrying out the conversion settings.
When you select the project, the area on the right shows the conversion target project setting items.
![](ProjectOperation_Eng-38.gif)
![](ProjectOperation_Eng-39.gif)
After setting the microcontroller to be used for the conversion target project, and project type, name, and place of creation settings, click the [OK] button.
If you select [Backup the project composition files after conversion], immediately after the conversion the project source files and complete project are packed up and saved. |
See "Project Convert Setting dialog box" for details about each setting item. |
The CubeSuite project is converted to the CS+ project.
A CubeSuite project is converted to a CS+ project according to the rule below.
A CubeSuite project is converted to a project with the same name as the original project. After conversion, the project file name will be "project name.mtpj". |
The project file after conversion is created in the folder the CubeSuite project file was placed in. If there is already a project file with the same name, "_number_" (number: 1, 2, ...) will be added to the file name. |
The build mode and build options information is not the target for conversion, if the build tool is different from the CubeSuite project file. |