The acquired floating license (offline mode) is automatically returned to the server when it expires. You can also manually end usage in the offline mode and return the floating license before it expires.
When the client is connected to the server, click the license name and the [Stop offline mode] button in the License Manger window.
![](LicenseManager_Eng-28.gif)
An floating license (offline mode) is returned to the server, and the displayed information in License Manager window is updated.
![](LicenseManager_Eng-29.gif)