3.5 When the Panel Is Opened during Execution of Program
The updated static analysis information will be displayed. The dynamic analysis information is not updated.
- | If this panel has been never opened since CS+ was launched: |
- | If this panel has been opened once since CS+ was launched: |
- | If this panel has been never opened since CS+ was launched:
The updated static analysis information will be displayed. The dynamic analysis information is not updated.
|
- | If this panel has been opened once since CS+ was launched:
The previous display contents will be displayed. |
The updated static analysis information will be displayed. The dynamic analysis information is not updated.
The previous display contents will be displayed.