Everything
2.9 Set Standard Library Generate Options

To set options for the library generator, select the Build tool node on the project tree and select the [Standard Library Generate Options] tab on the Property panel.

You can set the various library generate options by setting the necessary properties in this tab.

Caution

This tab is displayed in the following cases.

-

The project is for the other than library project.

-

[Always latest version which was installed] or V1.13.00 or a later version for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.13.00 or a later version of the CC-RL compiler has been installed