Start CSIH extended data reception by master mode.
This API function performs 2 byte-level CSIH reception the number of bots specified by the argument rx_bit_num, and stores the data in the buffer specified by the argument rx_buf. |
Starts after this API function is called, and R_CSIHm_Start is then called. |
#include "r_cg_macrodriver.h" MD_STATUS R_CSIHm_Master_Receive ( const uint16_t * rx_buf, uint16_t rx_bit_num, uint32_t chipId ); |