This section describes the API functions output by the Code Generator, using the following notation format.
![](cg_RH850api_e-1.gif)
Indicates the name of the API function.
Outlines the functions of the API function.
Indicates the format to be used when describing an API function to be called in C language.
API function arguments are explained in the following format.
API function return value is explained in the following format.