Everything

R_DCRAn_Input8bitData


Sets the calculation data for 8 bit width.

[Syntax]

void    R_DCRAn_Input32bitData ( const uint8_t * data, uint32_t data_num );

Remark

n is the unit number.

[Argument(s)]

I/O

Argument(s)

Description

I

const uint8_t * data;

Pointer to a buffer storing the calculation data

I

uint32_t data_num;

Total amount of calculation data

[Return value]

None.