R_DFE_Set_SoftwareData
Sets the data to be processed.in a target filter.
[Syntax]
void R_DFE_Set_SoftwareData ( uint8_t tag, int16_t const data );
[Argument(s)]
I/O
Argument(s)
Description
I
uint8_t tag;
Set the same value as the channel tag
int16_t const data;
Software input data
[Return value]
None.