R_DSADCm_GetResult
Reads the results of ΔΣ A/D conversion.
[Syntax]
void R_DSADCm_GetResult ( uint32_t * result );
Remark
m is the channel number.
[Argument(s)]
I/O
Argument(s)
Description
O
uint32_t * result;
Pointer to area in which to store the results of A/D conversion
[Return value]
None.