Sets the clock type (12-hour or 24-hour clock) of the real-time clock.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_rtc.h"
MD_STATUS R_RTC_Set_HourSystem ( rtc_hour_system_t hour_system );
|
[Argument(s)]
|
|
|
|
rtc_hour_system_t hour_system;
|
Clock type
HOUR12: 12-hour clock
HOUR24: 24-hour clock
|
[Return value]
|
|
MD_OK
|
Normal completion
|
MD_BUSY1
|
Executing count process (before change to setting)
|
MD_BUSY2
|
Stopping count process (after change to setting)
|
MD_ARGERROR
|
Invalid argument specification
|
Remark | If MD_BUSY1 or MD_BUSY2 is returned, it may be because the counter-operation is stopped, or the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger. |