Everything

r_uartm_callback_error


Performs processing in response to the UART error interrupt.

Remark

This API function is called as the callback routine of interrupt process r_uartm_interrupt_errorcorresponding to the UART error interrupt.

[Syntax]

#include    "r_cg_macrodriver.h"
void    r_uartm_callback_error ( uint8_t err_type );

Remark

m is the channel number.

[Argument(s)]

I/O

Argument(s)

Description

O

uint8_t err_type;

Trigger for UART error interrupt

0x00xx01B: Bit error

0x00x10xB: Overrun error

0x001x0xB: Framing error

0100xx0xB: Parity error

[Return value]

None.