Voltage detection circuit (LVDA)
Below is a list of API functions output by the Code Generator for voltage detection circuit use.
Table 3.3 API Functions: [Voltage Detection Circuit]
API Function Name |
Function |
Performs initialization necessary to control the voltage detection circuit. | |
Performs user-defined initialization relating to the voltage detection circuit. | |
Performs processing in response to the voltage monitoring n interrupt. | |
Starts voltage monitoring (when in interrupt mode, and interrupt & reset mode). | |
Ends voltage monitoring (when in interrupt mode, and interrupt & reset mode). |