Everything

Main window

Outline
This is the first window to be open when CubeSuite+ is launched.
This window is used to control the user program execution and open panels for the build process.
This window can be opened as follows:
- Select Windows [start] -> [All programs] -> [Renesas Electronics CubeSuite+] -> [CubeSuite+]
Display image
Explanation of each area
1 ) Menu bar
Displays the menus relate to realtime OS.
Contents of each menu can be customized in the User Setting dialog box.
- [View]
Realtime OS
The [View] menu shows the cascading menu to start the tools of realtime OS.
Resource Information
Opens the Realtime OS Resource Information panel.
Note that this menu is disabled when the debug tool is not connected.

2 ) Toolbar
Displays the buttons relate to realtime OS.
Buttons on the toolbar can be customized in the User Setting dialog box. You can also create a new toolbar in the same dialog box.
- Realtime OS toolbar
Opens the Realtime OS Resource Information panel.
Note that this button is disabled when the debug tool is not connected.

3 ) Panel display area
The following panels are displayed in this area.
- Output panel
See the each panel section for details of the contents of the display.
Note See "CubeSuite+ RX Build" for details about the Output panel.