20.19 Cyclic Handler Information (cyclic_hand[])
Here, each cyclic handler is defined.
Parentheses < >show the user input part.
- Description
Define the cyclic handler ID number.
- Definition format
Numeric value
- Definition range
From 1 to 255
- When omitting
The cfg600px assigns the ID number automatically.
- Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
#define <ID name> <ID number>
- Definition format
Symbol
- When omitting
Cannot be omitted.
3 ) Cyclic handler entry address (
entry_address)
- Description
Define the starting function of the cyclic handler.
- Definition format
Symbol
- When omitting
Cannot be omitted.
4 ) Activation cycle (
interval_counter)
- Description
Define the activation cycle in millisecond.
- Definition format
Numeric value
- Definition range
From 1 to (0x7FFFFFFF - system.tic_nume) / system.tic_deno
- When omitting
The set value in the default system configuration file (factory setting: 1) applied.
5 ) Initial state (
start)
- Description
Define the initial state of the cyclic handler.
- Definition format
Symbol
- Definition range
Select either of the following:
OFF: Non operational stat (The TA_STA attribute is not specified.)
ON: Operational state (The TA_STA attribute is specified.)
- When omitting
The set value in the default system configuration file (factory setting: "OFF") applied.
6 ) Activation phase (
phs_counter)
- Description
Define the activation phase in millisecond
- Definition format
Numeric value
- Definition range
From 0 to
interval_counter
- When omitting
The set value in the default system configuration file (factory setting: 0) applied.
7 ) TA_PHS attribute (
phsatr)
- Description
Define the attribute concerning the activation phase.
- Definition format
Symbol
- Definition range
Select either of the following:
OFF: Not preserve the activation phase. (The TA_PHS attribute is not specified.)
ON: Preserve the activation phase. (The TA_PHS attribute is specified.)
- When omitting
The set value in the default system configuration file (factory setting: "OFF") applied.
8 ) Extended information (
exinf)
- Description
Define the extended information of the cyclic handler.
- Definition format
Numeric value
- Definition range
From 0 to 0xFFFFFFFF
- When omitting
The set value in the default system configuration file (factory setting: 0) applied.
- Note
The extended information is passed to the cyclic handler.