ploc_mtx
ER ploc_mtx (ID mtxid);
If the target mutex could not be locked (another task has been locked) when this service call is issued but "E_TMOUT" is returned.
When the mutex is locked, this service call changes the current priority of the invoking task to the ceiling priority of the target mutex. However, this service call does not change the current priority when the invoking task has locked other mutexes and the ceiling priority of the target mutex is lower than or equal to the ceiling priority of the locked mutexes.
Note This service call returns "E_ILUSE" if this service call is re-issued for the mutex that has been locked by the invoking task (multiple-locking of mutex).