psnd_mbf
ipsnd_mbf
ER psnd_mbf (ID mbfid, VP msg, UINT msgsz);
ER ipsnd_mbf (ID mbfid, VP msg, UINT msgsz);
 These service calls process as follows according to the situation of the message buffer specified by the parameter mbfid.
 -	 There is a task in the reception wait queue.
This service call transfers the message specified by parameter msg to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (message reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
This service call transfers the message specified by parameter msg to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (message reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
 -	 There is no task neither in the reception wait queue and transmission wait queue and there is available space in the message buffer.
This service call stores the message specified by parameter msg to the message buffer. As a result, the size of available space in the target message buffer decreases by the amount calculated by the following expression.
This service call stores the message specified by parameter msg to the message buffer. As a result, the size of available space in the target message buffer decreases by the amount calculated by the following expression.
 -	 There is no task neither in the reception wait queue and transmission wait queue and there is no available space in the message buffer, or there is a task in the transmission wait queue.
These service calls return "E_TMOUT".
These service calls return "E_TMOUT".
 Note	 Message is written to the message buffer area in the order of the message transmission request.