tget_mpf
ER tget_mpf (ID mpfid, VP *p_blk, TMO tmout);
This service call acquires the fixed-sized memory block from the fixed-sized memory pool specified by parameter mpfid and stores the start address in the area specified by parameter p_blk.
If no fixed-size memory blocks could be acquired from the target fixed-size memory pool (no available fixed-size memory blocks exist) when this service call is issued, this service call does not acquire the fixed-size memory block but queues the invoking task to the target fixed-size memory pool wait queue and moves it from the RUNNING state to the WAITING state with time-out (fixed-size memory block acquisition wait state).
A fixed-sized memory block was returned to the target fixed-sized memory pool as a result of issuing rel_mpf.
|
|
A fixed-sized memory block was returned to the target fixed-sized memory pool as a result of issuing irel_mpf.
|
|
Note 1 Invoking tasks are queued to the target fixed-size memory pool wait queue in the order defined at creating the fixed-sized memory pool. (FIFO order or current priority order).
Note 3 The alignment number of memory block is 1. Please perform the following, in order to enlarge the alignment number of memory blocks.
- Specify the memory block size to a multiple of the desired alignment number at creating the fixed-sized memory pool.
- Make the start address of the fixed-sized memory pool area into the address of the desired alignment number.
Note 4 TMO_FEVR is specified for wait time tmout, processing equivalent to get_mpf will be executed. When TMO_POL is specified, processing equivalent to pget_mpf will be executed.