tsnd_dtq
ER tsnd_dtq (ID dtqid, VP_INT data, TMO tmout);
This service call processes as follows according to the situation of the data queue specified by the parameter dtqid.
- There is a task in the reception wait queue.
This service call transfers the data specified by parameter data to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
This service call transfers the data specified by parameter data to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
- There is no task neither in the reception wait queue and transmission wait queue and there is available space in the data queue.
This service call stores the data specified by parameter data to the data queue.
This service call stores the data specified by parameter data to the data queue.
- There is no task neither in the reception wait queue and transmission wait queue and there is no available space in the data queue, or there is a task in the transmission wait queue.
This service call queues the invoking task to the transmission wait queue of the target data queue and moves it from the RUNNING state to the WAITING state with time (data transmission wait state).
The sending WAITING state for a data queue is cancelled in the following cases.
This service call queues the invoking task to the transmission wait queue of the target data queue and moves it from the RUNNING state to the WAITING state with time (data transmission wait state).
The sending WAITING state for a data queue is cancelled in the following cases.
Note 1 Data is written to the data queue area of the target data queue in the order of the data transmission request.
Note 2 Invoking tasks are queued to the transmission wait queue of the target data queue in the order specified at creating the data queue (FIFO order or current priority order).
Note 3 TMO_FEVR is specified for wait time tmout, processing equivalent to snd_dtq will be executed. When TMO_POL is specified, processing equivalent to psnd_dtq will be executed.