can_act
ican_act
ER_UINT can_act (ID tskid);
ER_UINT ican_act (ID tskid);
This service call cancels all of the activation requests queued to the task specified by parameter tskid (sets the activation request counter to 0).
When this service call is terminated normally, the number of cancelled activation requests is returned.
Note This service call does not perform status manipulation processing but performs the setting of activation request counter. Therefore, the task does not move from a state such as the READY state to the DORMANT state.