CHAPTER 17 DATA TYPES AND MACROS
This chapter describes the data types and macros, which are used when issuing service calls provided by the RI600V4.
Note <ri_root> indicates the installation folder of RI600V4.
The default folder is "C:\Program Files\Renesas Electronics\CubeSuite+\RI600V4".
The default folder is "C:\Program Files\Renesas Electronics\CubeSuite+\RI600V4".
Macro definition of the data type is performed by <ri_root>\in600\kernel.h, or <ri_root>\inc600\itron.h that is included by kernel.h.
This section explains the macros (for current state, processing program attributes, or the like) used when issuing a service call provided by the RI600V4.
- System information header file kernel_id.h, which is generated by the cfg600.
The contents of this file is changed according to the system configuration file.
The contents of this file is changed according to the system configuration file.
3 ) ER ERCD ( ER mercd, ER sercd )
Return the error code from the main error code indicated by mercd and sub error code indicated by sercd.
Return the error code from the main error code indicated by mercd and sub error code indicated by sercd.
Note In the error code returned from the RI600V4, all sub error code is -1, and all main error code is same as the value described in Table 17-2.