pol_flg
ipol_flg
ER pol_flg (ID flgid, FLGPTN waiptn, MODE wfmode, FLGPTN *p_flgptn);
ER ipol_flg (ID flgid, FLGPTN waiptn, MODE wfmode, FLGPTN *p_flgptn);
This service call checks whether the bit pattern specified by parameter waiptn and the bit pattern that satisfies the required condition specified by parameter wfmode are set to the eventflag specified by parameter flgid.
If the bit pattern that satisfies the required condition has been set to the target eventflag, the bit pattern of the target eventflag is stored in the area specified by parameter p_flgptn.
If the bit pattern of the target eventflag does not satisfy the required condition when this service call is issued, "E_TMOUT" is returned.
- wfmode == TWF_ANDW
Checks whether all of the bits to which 1 is set by parameter waiptn are set as the target eventflag.
Checks whether all of the bits to which 1 is set by parameter waiptn are set as the target eventflag.
- wfmode == TWF_ORW
Checks which bit, among bits to which 1 is set by parameter waiptn, is set as the target eventflag.
Checks which bit, among bits to which 1 is set by parameter waiptn, is set as the target eventflag.
Note 1 With the RI600V4, whether to enable queuing of multiple tasks to the event flag wait queue is defined during configuration. If this service call is issued for the event flag (TA_WSGL attribute) to which a wait task is queued, therefore, "E_ILUSE" is returned regardless of whether the required condition is immediately satisfied.
Note 2 The RI600V4 performs bit pattern clear processing (0 setting) when the required condition of the target eventflag (TA_CLR attribute) is satisfied.