Everything

tget_mpl

Outline
Acquire variable-sized memory block (with time-out).
C format
 ER      tget_mpl (ID mplid, UINT blksz, VP *p_blk, TMO tmout);
Parameter(s)
I/O
Parameter
Description
I
 ID      mplid;
ID number of the variable-sized memory pool.
I
 UINT    blksz;
Memory block size to be acquired (in bytes).
O
 VP      *p_blk;
Start address of the acquired memory block.
I
 TMO     tmout;
Specified time-out (in millisecond).
TMO_FEVR: Waiting forever.
TMO_POL: Polling.
Value: Specified time-out.

Explanation
This service call acquires a variable-size memory block of the size specified by parameter blksz from the variable-size memory pool specified by parameter mplid, and stores its start address into the area specified by parameter p_blk.
If no variable-size memory blocks could be acquired from the target variable-size memory pool (no successive areas equivalent to the requested size were available) when this service call is issued, this service call does not acquire variable-size memory blocks but queues the invoking task to the target variable-size memory pool wait queue and moves it from the RUNNING state to the WAITING state with time-out (variable-size memory block acquisition wait state).
The WAITING state for a variable-sized memory block is cancelled in the following cases.
WAITING State for a Variable-sized Memory Block Cancel Operation
Return Value
The variable-size memory block that satisfies the requested size was returned to the target variable-size memory pool as a result of issuing rel_mpl.
E_OK
The task at the top of the transmission wait queue was forcedly released from waiting by following either.
- Forced release from waiting (accept rel_wai while waiting).
- Forced release from waiting (accept irel_wai while waiting).
- Forced release from waiting (accept ter_tsk while waiting).
- The time specified by tmout for tget_mpl has elapsed.
E_OK
Forced release from waiting (accept rel_wai while waiting).
E_RLWAI
Forced release from waiting (accept irel_wai while waiting).
E_RLWAI
The variable-sized memory pool is reset as a result of issuing vrst_mpl.
EV_RST
The time specified by tmout has elapsed.
E_TMOUT

Note 1 For the size of the memory block, refer to "7.3.2 Size of Variable-sized memory block".
Note 2 Invoking tasks are queued to the target variable-size memory pool wait queue in the FIFO order.
Note 3 The contents of the block are undefined.
Note 4 The alignment number of memory blocks is 1. To enlarge the alignment number to 4, specify unique section to Section name assigned to the memory pool area (mpl_section) in Variable-sized Memory Pool Information (variable_memorypool[]) and locate the section to 4-bytes boundary address when linking.
Note 5 TMO_FEVR is specified for wait time tmout, processing equivalent to get_mpl will be executed. When TMO_POL is specified, processing equivalent to pget_mpl will be executed.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_PAR
-17
Parameter error.
- blksz == 0
- blksz exceeds the maximum size that can be acquired.
- tmout < -1
- tmout > (0x7FFFFFFF - TIC_NUME) / TIC_DENO
E_ID
-18
Invalid ID number.
- mplid < 0
- mplid > VTMAX_MPL
E_CTX
-25
Context error.
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the dispatching disabled state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_RLWAI
-49
Forced release from the WAITING state.
- Accept rel_wai/irel_wai while waiting.
E_TMOUT
-50
Polling failure or specified time has elapsed.
EV_RST
-127
Released from WAITING state by the object reset (vrst_mpl)