Everything

tslp_tsk

Outline
Put task to sleep (with time-out).
C format
 ER      tslp_tsk (TMO tmout);
Parameter(s)
I/O
Parameter
Description
I
 TMO     tmout;
Specified time-out (in millisecond).
TMO_FEVR: Waiting forever.
TMO_POL: Polling.
Value: Specified time-out.

Explanation
This service call moves the invoking task from the RUNNING state to the WAITING state (sleeping state).
As a result, the invoking task is unlinked from the ready queue and excluded from the RI600V4 scheduling subject.
If a wake-up request has been queued to the target task (the wake-up request counter > 0) when this service call is issued, this service call does not move the state but decrements the wake-up request counter (by subtracting 1 from the wake-up request counter).
The sleeping state is cancelled in the following cases.
Sleeping State Cancel Operation
Return Value
A wake-up request was issued as a result of issuing wup_tsk.
E_OK
A wake-up request was issued as a result of issuing iwup_tsk.
E_OK
Forced release from waiting (accept rel_wai while waiting).
E_RLWAI
Forced release from waiting (accept irel_wai while waiting).
E_RLWAI
The time specified by tmout has elapsed.
E_TMOUT

Note When TMO_FEVR is specified for wait time tmout, processing equivalent to slp_tsk will be executed.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_PAR
-17
Parameter error.
- tmout < -1
- tmout > (0x7FFFFFFF - TIC_NUME) / TIC_DENO
E_CTX
-25
Context error.
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the dispatching disabled state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_RLWAI
-49
Forced release from the WAITING state.
- Accept rel_wai/irel_wai while waiting.
E_TMOUT
-50
Polling failure or specified time has elapsed.