vrst_mpf
ER vrst_mpf (ID mpfid);
The tasks to wait to get memory block from the target fixed-sized memory pool are released from the WAITING state, and EV_RST is returned as a return value for the tasks.
Note 1 All fixed-sized memory blocks that had already been acquired are returned to the target fixed-sized memory pool. Therefore, do not access those fixed-sized memory blocks after issuing this service call.