This option performs optimization on the areas that are allocated before the execution start symbol.
Optimization is not performed on any area allocated before the execution start symbol.
This option performs optimization on the areas that are allocated before the execution start symbol. |
Specifying this option more than once has the same effect as specifying it once only. A warning is output in this case. |
If an address is specified by the -entry option, this option outputs a warning and ignores the specification. |
To perform optimization including the areas that are allocated before the execution start symbol, describe as: |