This option specifies the use of a subcommand file to specify the assemble options to be passed to the assembler.
Only the assemble options specified by the compilation driver are passed to the assembler.
This option specifies the use of subcommand file file to specify the assemble options to be passed to the assembler. |
To specify the use of subcommand file "command_asm.txt" to specify the assemble options to be passed to the assembler. |