This option specifies the use of a subcommand file to specify the link options to be passed to the optimizing linker.
Only the link options specified by the compilation driver are passed to the optimizing linker.
This option specifies the use of subcommand file file to specify the link options to be passed to the optimizing linker. |
To specify the use of subcommand file "command_lnk.txt" to specify the link options to be passed to the optimizing linker. |