This option specifies the input binary file.
This option specifies input binary file file. |
If the extension is omitted from the input file specification, it is assumed that ".bin" has been specified. |
Input binary data is allocated as the data of specified section section. |
When symbol symbol is specified, it can be linked as a defined symbol. |
The section specified by this option can have its section attribute and number of alignment specified. |
If attribute is omitted, the write, read, and execute attributes will be all valid by default. [V1.04 or earlier]
CALLT0, CODE, TEXT, TEXTF, TEXTF_UNIT64KP, CONST, CONSTF, SDATA, DATA, DATAF, OPT_BYTE, or SECUR_ID can be specified as the section attribute attribute. CODE becomes the same as the relocation attribute of TEXT. If a name other than ".option_byte" is specified for the section name while OPT_BYTE is specified, an error will occur. If a name other than ".security_id" is specified for the section name while SECUR_ID is specified, an error will occur. |
If attribute is omitted, the write, read, and execute attributes will all be valid by default. [V1.05 or later]
The value that can be specified for number of alignment alignment is a power of 2 (1, 2, 4, 8, 16, or 32). |
The binary file specified by this option can be allocated to only addresses 0 to 0x0FFFF. [V1.04 or earlier] |
b.bin is allocated from 0x200 as the .D1bin section. |