This option allows a library to be generated from multiple same module names.
This option allows multiple input files with the same module name to be specified to generate a library. |
If the library already contains a module having the same name with other modules to be registered in the library, the other modules are renamed by adding a postfix number ".<N>". |
<N> is assigned a number as a unique module name in the generating library. If can't assigned a unique number, The linker will output the error message and quit. |
To generate a library a.lib from multiple input files having the same module name (mod), describe as: |
The command line above leads to generate a library a.lib containing the following modules:
If the -form={ object|absolute|relocate|hexadecimal|stype|binary }, -strip, or -extract option is specified, this option will be invalid. |