Everything

-head


This option specifies the library to be configured.

[Specification format]

-head=<sub>[,...]
<sub> : { all | runtime | ctype | math | mathf | stdio | stdlib | string | inttypes }

 

-

Interpretation when omitted

It is the same result as when -head=all is specified.

[Detailed description]

-

This option specifies a library to be configured with a header file name.

-

If -head=all is specified, all header file names are specified as those to be configured.

-

Runtime libraries are always configured.