Everything
2.5.4 Library generator options [V1.13.00 or later]

 

This section explains options for the library generation phase.

Table 2.10

Library Generator Options

Classification

Option

Description

Library generation control

-head

This option specifies the library to be configured.

-lang

This option specifies the language standard of the standard library.

-secure_malloc [Professional Edition only]

This option generates a malloc library for security facility.

Output control

-output

This option specifies the output file name.

Other

-logo / -nologo

This option controls the copyright display.

-subcommand

This option specifies the subcommand file.