Compile options that can be specified for the library generator
In addition to library options, compile options can be specified for the library generator so that they can be selected when compiling a library.
The following compile options can be specified for the library generator. If any other compile option is specified, an error occurs or the specification is ignored without a warning output.
Make sure that the specifications of these options are the same as those for the application programs that reference the library. Library-specific specifications of some options are possible. Such options are indicated in the "Individual specification" column.
For details about each option, see "2.5.1 Compile options".