If show=cfi is specified, this option outputs the contents of the function list for use in detecting illegal indirect function calls.
The output example is given below.
*** CFI Table List *** SYMBOL/ADDRESS _func (1) 0000F100 (2) |
|
Outputs the address of the function if a symbol for it has not been defined. |