When the -show=xreference option is specified, the reference information of symbols (cross reference information) is output.
The output example of the cross reference information is shown below.
*** Cross Reference List *** (1) (2) (3) (4) (5) No Unit Name Global.Symbol Location External Information 0001 sample1 SECTION=.text _main 00000100 _func_01 00000118 SECTION=.data _gval3 000f0400 0003(00000032:.text) 0003(00000038:.text) SECTION=.bss _gval1 000f0404 0001(0000001a:.text) 0001(00000020:.text) _gval2 000f0408 0002(00000026:.text) 0002(0000002c:.text) 0002 sample2 SECTION=.text _func02 00000124 0001(0000000a:.text) 0003 sample3 SECTION=.text _func03 00000130 0001(00000010:.text) |