Source Options
< Compile Options / Source Options >
The following source options are available.
-
-lang
-include
-preinclude
-define
-undefine
-message
-nomessage
-change_message
-no_warning [V2.08.00 or later]
-file_inline_path
-comment
-truncated_address_initializer [V3.01.00 or later]
-check
-misra2004 [Professional Edition only]
-misra2012 [Professional Edition only] [V2.04.00 or later]
-ignore_files_misra [Professional Edition only]
-check_language_extension [Professional Edition only]
-misra_intermodule [Professional Edition only] [V3.01.00 or later]