Everything

-comment


< Compile Options / Source Options >

[Format]

-comment = { nest | nonest }

[Description]

-

When comment=nest is specified, nested comments are allowed to be written in the source file.

-

The default for this option is comment=nonest.

-

When comment=nonest is specified, comment nesting is not recognized.

[Example]

-

When comment=nest is specified, the compiler handles the above line as a nested comment; however, when comment=nonest is specified, the compiler assumes (1) as the end of the comment.

/* This is an example of /* nested */ comment */
                                  (1)