Everything

-define


< Assembler Command Options / Source Options >

[Format]

-define=<sub>[,...]
        <sub>: <macro name> = <string>

[Description]

-

This option replaces the macro name with the specified string.
(This provides the same function as writing the .DEFINE directive at the beginning of the source file.)

[Remarks]

-

.DEFINE takes priority over the define option if both are specified.