< Assembler Command Options / Source Options >
[Format]
[Description]
- | This option outputs warning W0551013 when a DSP instruction is written in the source file. |
[Remarks]
- | For details of the DSP instructions, refer to the RX Family Software Manual. |