Everything

-patch


< Assembler Command Options / Microcontroller Options >

[Format]

-patch = { rx610 }

[Description]

-

This option is used to avoid a problem specific to the CPU type.

-

When -patch=rx610 is specified, the MVTIPL instruction which causes a problem in the RX610 Group is handled as an undefined instruction. The MVTIPL instruction will not be recognized as an instruction and the error message E0552113 will be output.