< Assembler Command Options / Microcontroller Options >
[Format]
[Description]
-  | This option is used to avoid a problem specific to the CPU type.  | 
 
-  | When -patch=rx610 is specified, the MVTIPL instruction which causes a problem in the RX610 Group is handled as an undefined instruction. The MVTIPL instruction will not be recognized as an instruction and the error message E0552113 will be output.  |